Reset the default admin password
If the default administrator (
piadmin
) password is lost or forgotten and you cannot make administrator-level changes to FactoryTalk Historian ME, you must reset the piadmin
user password and security settings.To reset the default admin password
- Click theAdvancedtab, and then clickRestore Defaults.TheRestore Defaultspage appears.
- ClickReset Security.A message appears asking you to confirm the action.
- ClickOK.
You can now access default administrator functions. The default password for the
piadmin
user is empty. It is important to change the default piadmin
password after you log on.
TIP:
You can also reset the password from the Logix Designer interface. For details, see Configure the module properties.
Provide Feedback