View and edit the current time
To view and edit the current time in FactoryTalk Historian ME
- Click theAdvancedtab, and then clickTime Management.TheTime Managementpage appears.You can view the module's current time in theModule's Current Timebox.
- Select one of the time synchronization options:
- Controller TimeIn the list, select a controller or a shortcut to a local controller which will be used for time synchronization.TIP:The Logix Designer installation DVD contains the Logix Designer Clock Update Tool. The tool lets you view and synchronize the system time of the controllers and devices on a network, using any computer with a Microsoft Windows operating system and RSLinx Classic installed. For details, see the Logix Designer Clock Update Tool online help.If you use a shortcut to a local controller as the time source, and this shortcut or the controller to which the shortcut is pointing is removed, an error message appears informing you that this time source is no longer available.
- NTP ServerIn the box, type the IP address or the hostname of the NTP server computer which will be used for the time synchronization.For details on using this option, see Considerations for using an NTP server as the time source.
- Manual SetIn the box, type the new time in the same format as the one displayed in theModule's Current Timebox. The time is kept by the module's real-time clock.TIP:With this option selected, the module's time is not synchronized with any time source. As it may result in a potential drift of the real-time clock over time, theManual Setoption should only be used in rare cases such as demonstrations or troubleshooting associated with maintenance.For details, see Clock drifts.
- ClickSave.The module is automatically rebooted, and the updated time is displayed in theModule's Current Timebox.TIP:The time on the selected time source may be in the past compared to the current module time. Using such a time source will cause the module time to be in the past, and will cause the module to reboot into safe mode. In such a case, you need to repair the archive files and get the module out of safe mode.For details, see Repair archives using safe mode.
Provide Feedback