Configure network settings
TIP:
You must have administrator privileges to configure network settings.
To configure network settings
- ClickAdvanced, and then clickSystem Settings.TheSystem Settingspage appears.
- Review the following for additional information.ItemDescriptionConfigurationSelect Dynamic Host Configuration Protocol (DHCP) or Static IP. DHCP is selected by default.DHCPLeave this option selected to automate the network parameter assignment to network devices from one or more DHCP servers.A DHCP server is required to assign the module its initial IP address. Note that the Logix Designer DHCP Server tool can be used to set the IP address.Static IP AddressSelect this option to use the same IP address every time the module powers up.If you type an IP address that is already in use and then reboot the module, you will not be able to access the module through the web interface. To repair this, access the module through FactoryTalk Historian ME Logix Designer Module Profile and reset the network configuration. For details, see Use Studio 5000 Logix Designer Module Profile.IP AddressThe module's IP address.Make sure that the IP address you use is not assigned to another device in your network.This field is enabled when you selectStatic IP Address.MAC AddressThe module's Media Access Control (MAC) address.The address comes from the module and cannot be changed.Subnet MaskThe module's subnet mask.The value is unique to your location. To get the correct value, consult your IT department.This field is enabled when you selectStatic IP Address.Default GatewayThe network default gateway.This allows data to be passed from one subnet to another in a network.This field is enabled when you selectStatic IP Address.Search DomainThe DNS search domain.This field is enabled when you selectStatic IP Address.Primary DNS ServerThe first Domain Name System (DNS) server.This field is enabled when you selectStatic IP Address.Secondary DNS Server(optional) The secondary DNS server.This field is enabled when you selectStatic IP Address.Auto-NegotiateSelect this check box if you want the Autonegotiation to determine the speed and duplex parameters. The speed and duplex parameters must match the parameters on the router switch.SpeedThe network speed. Ensure that this setting matches the speed set on the switch port that your module is connected to.This field is enabled when theAuto-Negotiatecheckbox is not selected.DuplexThe duplex parameter determines how communication is sent and received.
- In the list, selectFullif you want both communications ends to be able to send and receive signals at the same time.
- In the list, selectHalfif you want the communication to be bidirectional. However, note that the signals can only flow in one direction at a time.
Ensure that this setting matches the speed set on the switch port that your module is connected to.This field is enabled when theAuto-Negotiatecheckbox is not selected. - ClickSave.A message appears asking you to confirm that you want to change the settings.
- ClickOK.TIP:If you change the default IP address configuration from DHCP to Static IP Address, or if you use BootP through Logix Designer and a BOOTP/DHCP server, you cannot access the module using its host name. The new IP address is not associated with the module hostname on the DNS server, and the hostname does not resolve. To avoid this issue, consult your local IT department to register the new IP address with the DNS server.
Provide Feedback