Reboot the module
To reboot the module
- Click theAdvancedtab, and then clickModule Shutdown.
- UnderModule Reboot, clickModule Reboot.A message appears asking you to confirm the action.
- ClickOK.TIP:Alternatively, you can reboot the module using the FactoryTalk Historian ME Logix Designer Module Profile.If the Restore Defaults or Reset Security actions are being executed on your Historian module in the Logix Designer Module Profile, you will not be able to restore the default settings, reset the security configuration, or reboot the module from the web client.For details, see Configure the module properties.
Provide Feedback