View the backup status and perform backup

To view the backup status
  1. Click the
    Configure Historian
    tab, and then click
    Backup And Restore
    .
    The
    Backup and Restore
    page appears.
  2. Under
    Backup Status
    , view the details of the most recent backup of the system configuration:
    • The status of the backup.
    • The date of the backup.
    • The name of the backup file.
    • The size of the backup file.
    The backup file contains configuration information for the following:
    • Data collection.
    • Data storage.
    • Data transfer.
    • Security.
    • Data server.
    • Point server.
    • Web server.
      TIP:
      If any changes have been made to the system configuration since the last backup, it is recommended to perform another backup.
  3. Click
    Backup
    to perform the system backup.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal