Network manager

Click the
Network Manager
option to view the current network manager connection statistics.
Network Manager - Chrome
The
Network Manager
section displays the following information:
Item
Description
ID
The connection ID. This is the primary key.
Path
The root directory on the server. This directory is the same for all connections.
Name
The connection name.
ID
The process ID number.
Reg App Name
The registered application name.
Reg App Type
The registered application type.
Protocol Version
The protocol version of connecting application.
Peer Name
The hostname of connecting machine.
Peer Address
The IP address of the connecting machine.
Peer Port
The port number of connecting machine.
ConType
The connection type.
Net Type
The network type.
ConStatus
The connection status.
ConTime
The time of the connection.
Last Call
The time of the last call.
Elapsed Time
The amount of time passed.
Bytes Sent
The number of bytes sent.
Bytes Recv
The number of bytes received.
Msg Sent
The number of messages sent.
Msg Recv
The number of messages received.
Errors Recv
The number of errors received.
Errors Sent
The number of errors sent.
API Count
The number of APIs.
SDK Count
The number of SDKs.
Server ID
The identification number of the server.
NetMgr Version
The number of the network manager version.
OS Sys Name
The operating system name.
OS Node Name
The operating system node name.
OS Release
The operating system release number.
OS Version
The operating system version number.
Machine
The system name.
User
The user name.
OS User
The operating system user name.
Trust
The name of the trust connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal