Point statistics

Point Statistics chart
The
Point Statistics
section displays information about points configured on the module in the form of statistics and a pie chart.
Review the following for additional information.
Item
Description
Total Points
The number of total points on the module.
Total Active Points
The number of points actively receiving data.
Incl. Bad Points
The number of points out of the Total Active Points which are configured for collecting data but are not actively receiving it because the point is being rejected by the data server with an error.
The pie chart rounds the percentage to the nearest whole percent. For instance, if there are 1000 total points in the system and 995 active points, the pie chart will still display 100%, but if there are 994 active points, the pie chart will display 99% and 1%.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal