Client connections

The
Client Connections
section displays the number of clients currently connected to FactoryTalk Historian ME. There may be up to 5 clients connected simultaneously to the Historian module.The following client applications are supported:
- FactoryTalk Historian DataLink
- FactoryTalk Historian ProcessBook
- FactoryTalk View SE Trending
- FactoryTalk Administration Console
- PI System Management Tools (SMT)
- FactoryTalk VantagePoint
- FactoryTalk VantagePoint EMI
Provide Feedback