View the module information

The module information is displayed on the following pages of the
Home
tab:
Additionally, there is also the System Status section in the left bottom corner of every page of the web client.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal