Bad quality data

FactoryTalk Historian ME
tracks data quality during the data collection and the data transfer. It may happen that data is of bad quality (for example, if the controller loses its connection to the
FactoryTalk Historian ME
, or if a running tag is removed from the controller but not from
FactoryTalk Historian ME
).
Bad quality data is displayed in the point list with the
Bad_Quality
value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal