Overview

The
Overview
page displays the following information:
Item
Description
CPU Usage
The percent of CPU utilization for the module.
RAM Usage
The RAM (physical memory) usage in megabytes (and percentage).
NAND Usage
NAND usage (storage) in megabytes (and percentage).
Ethernet Link
Displays the module's Ethernet connection status.
LED
Information for either the static or the scroll display will be available. If a static message is available, there is no scrolling display. If a message is scrolling in the module LED, no static message is available.
  • Static Display
    The current message being displayed on module LED.
  • Scroll Display
    The current message being scrolled on module LED.
Hardware overview
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal