EtherNet/IP
The
EtherNet/IP
page contains the following sections:- Network SettingsThis section displays the following information:ItemDescriptionLink StatusIndicates ifFactoryTalk Historian MEis connected to the Ethernet network.IP AddressTheFactoryTalk Historian MEIP address.Ethernet Access (MAC)TheFactoryTalk Historian MEMAC address.IP Configuration ModeIndicates the network setting used for theFactoryTalk Historian MEmodule.
- Network StatisticsThis section displays the following information:ItemDescriptionSent PacketsThe number of network packets sent per second.Received PacketsThe number of network packets received per second.Sent BytesThe number of bytes sent per second.Received BytesThe number of bytes received per second.Sent Packets CountThe cumulative number of total network packets sent.Received Packets CountThe cumulative number of total network packets received.

Provide Feedback