Display LED

The
Display LED
page displays the current message being displayed or scrolled on the module LED in further detail and the LED statistics.
The page lists
Current Display
and
LED Statistics
information. Data for either the static or the scroll display will be available. If a static message is available, there is no scrolling display. If a message is scrolling in the module LED, no static message is available.
Item
Description
LED Static Display
The current message being displayed on the module LED.
LED Scroll Display
The current message being scrolled on the module LED.
The Display LED page lists the Application LED State information under
LED Statistics
. Values include:
Item
Description
Solid green
Indicates that both data collection and data transfer are active.
Flashing green
Indicates that the data collection is active but the data transfer is not configured.
Solid red
Indicates that the data collection is inactive.
Flashing red
Indicates that the data collection is active but the data transfer is inactive.
Display LED
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal