Overview
The
Overview
page displays the following information:Item | Description |
|---|---|
Component Status | Displays the current status of all firmware components, either Running or Stopped. |
Security Mode | Displays the current security mode, either FactoryTalk Historian ME Local Security or FactoryTalk Directory Security. |
Last Backup | Displays status, date, file name, and file size of the last backup. |
Top Processes | Displays the running processes in descending order based on CPU usage. |
Provide Feedback