Data transfer

The
Data Transfer
page lists the following information:
Item
Description
Process Name
The title of the process.
CPU Usage
The percent of CPU utilization.
Memory Used
The amount of memory (in megabytes) utilized by the data transfer service.
Up Time
The amount of CPU time used.
Priority
Indicates the precedence order for the process.
Nice Value
A value that indicates the CPU process priority. The default value is zero. A high Nice value indicates a lower priority for the process. Negative Nice values are a higher priority.
Transfer Rate
The current transfer rate from the data transfer service in events per minute.
Successful Attempt Rate
The number of attempts to transfer data to the FactoryTalk Historian SE or PI server per hour.
Data Transfer
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal