Data server
The
Data Server
page displays the Data Server process name, CPU usage, memory used, uptime, priority, and Nice value.The page lists the following information:
Item | Description |
|---|---|
Process Name | The title of the process. |
CPU Usage | The percent of CPU utilization. |
Memory Used | The amount of memory (in megabytes) utilized by the data server. |
Up Time | The amount of CPU time used. |
Priority | Indicates the precedence order for the process. |
Nice Value | A value that indicates the CPU process priority. The default value is zero. A high Nice value indicates a lower priority for the process. Negative Nice values are a higher priority. |

Provide Feedback