Restart services
The
Restart Service
page allows you to:Item | Description |
|---|---|
Restart web | Click this button to restart the web configuration server process. Please note that the restart is done without authentication. |
Restart CIP | Click this button to reset the CIP process. Please note that the restart is done without authentication. |
Restart Data Transfer | Click this button to restart the data transfer. Please note that the restart is done without authentication. |
Module Reboot | Click this button to reboot the entire module after restarting any service. |
Provide Feedback