Configure your Historian module in the Module Profile
To configure the Historian module in the Module Profile
- Add the Historian module to a project in Logix Designer.
- Add the Ladder logic to the controller.For details, see Example: Use the Module Profile.
Provide Feedback