Point server issues
Symptom | Solution |
|---|---|
The System Status section on the Home page shows that the Point Server is in the "Error" mode. | This indicates the Point Server is in an undesirable state. Restart the module. |
Provide Feedback