Start the data transfer

To start the data transfer
  1. Click the
    Configure Historian
    tab, and then click
    Data Transfer
    .
  2. Under
    Data Transfer Parameters
    , click
    Start
    .
    The status changes from
    Stopped
    to
    Running
    .
    If the
    FactoryTalk Historian SE
    or PI server becomes unavailable, the data will continue to be stored on the module. When the server becomes available again, it will automatically reconnect, and the data transfer will continue.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal