SNMP community strings
The Simple Network Management Protocol (SNMP) is a protocol for communication between devices connected in a network. SNMP uses community strings as passwords that allow a get-request to access the statistics of a module.
TIP:
- The Backup and Restore function does not include the SNMP community strings.
- Restoring FactoryTalk Historian ME defaults disables SNMP and deletes the existing community strings. The system creates the default community string:public.
Provide Feedback