Add the Historian ME module in the PI SDK Utility
To add the Historian ME module in the PI SDK Utility
- Go toStart > All Programs > Rockwell Software > FactoryTalk Historian SE > FactoryTalk Historian SE System > About PI-SDK.ThePI SDK Utilitywindow appears.
- On theFilemenu, clickConnections.ThePI Connection Managerdialog box appears.
- On theServermenu, clickAdd server.TheAdd PI Serverdialog box appears.
- In theNetwork Path/FQDNbox, type the IP address of the Historian module.
- ClickOK.If a connection was successfully established, the IP address will appear in thePI Connection Managerdialog box. If an error occurs, the module might be restarting. Ensure that the middle STS LED is flashing green on the module. This indicates that the module has fully initialized and a connection can be established.
Provide Feedback