Add points using the Add Individual Points page
To add points using the Add Individual Points page
- ClickManage Points, and then clickAdd Individual Points.TheAdd Individual Pointspage appears.
- In theTag Filelist, select a tag attribute file. The default isFTHMETagDefault.xml.The tag attribute file defines the attributes of the points to be created.To view the content of the file, click
next to the list.Rule files are managed through theRule Editor. For details, see Use the rule editor. - In theScan Ratelist, do either of the following:
- If you want to set a global scan rate, select a value in seconds.The scan rate defines how frequently the data is collected.Points with invalid scan rates will not be created.For tags, the maximum number of events per second is 2500. For the data collection rates slower than 500ms, use Polled and Advised tags.The valid scan rates are the following:For this scan typeUse this scan rate
- Advised
- Polled
Equal to or greater than 0.5 seconds.- High-speed
Equal to or greater than 0.01 seconds, and equal to or less than 0.5 seconds. - If you use multiple tag attribute files that define different scan rates and you want to use these scan rates rather than a global one, selectdefault.
- UnderFolders, expand the tree, and select the controller from which you want to use tags.The controller's tags are displayed underContents.To refresh the list of controllers, clickRefresh.
- (optional) To further filter the tag search results, filter the tags using theTag Filterbox belowFolders:
- In theTag Filterbox, type a tag name or a part of a tag name with *, and then pressEnter.The tags that are displayed underContentsare filtered using the filter criteria that you have specified in theTag Filterbox.To display all the tags again with no filter applied, type * in theTag Filterbox, and then pressEnter.
- UnderContents, select the tags that you want to use to create points.To select all the tags, select theAll/Nonecheckbox belowContents.
- ClickAdd Tag(s) to List.The tags that you have selected are listed in theSelected Tagstable.
- ClickCreate, and confirm the action in the message box that appears.The points are created.The following information is displayed:
- The number of points that were created based on the tags that you have selected.
- The number of points that were not created because of either of the following reasons:
- A specific point already exists in the archive.
- An error occurred.For details, see System log related issues.
- The total number of points in the module, including the newly created ones.
The points that have not been created are listed in the
Points Not Created
table, along with an explanation for the point creation failure.Once you finalize the data point creation, restart the data collection by clicking
Restart Data Collection
. The process may take several minutes.Provide Feedback