Create shortcuts to a remote controller
When creating shortcuts to remote controllers, take into consideration the following points:
- The remote controller should be located in a local area network (LAN) rather than a wide area network (WAN) or a low-speed network.
- You can create up to 5 shortcuts to remote controllers.
- The shortcut paths must be unique. This means that each shortcut must point to a different controller or have a different CIP path.
To create a shortcut to a remote controller
- ClickManage Points, and then clickManage Shortcuts.
- ClickAdd.
- UnderAdd New Shortcut, clickRemote controller.
- Select a local communication module.
- Type the IP address of a remote communication module, and then clickLoad Controllers.Controllers will not be loaded if:
- The IP address is incorrect.
- There are no supported controllers detected in the remote chassis.TIP:For a list of supported controllers, refer to the FactoryTalk Historian ME Release Notes.
- Select the remote controller to which you want to create the shortcut.Alternatively, select theAdd the shortcut using a CIP path insteadoption, and type the CIP path to the controller.
- Type the name of the shortcut.When typing the name, take into consideration the following points:
- The name can contain only the characters a-z, A-Z, 0-9, and an underscore.TIP:To learn about the convention of naming tags added to the Historian module using the shortcuts, see Tag naming conventions.
- The maximum length of the name is 40 characters.TIP:To minimize the complexity of tag names, we recommend that you keep the shortcut names short.
- The name must start with a letter or an underscore.
- The name cannot contain two underscores side by side, or an underscore with a number at the end of the name (for example, shortcut_12).
- The shortcut name must be unique.
- ClickSave.The shortcut is added to the shortcut table.TIP:If any error occurs when creating the shortcut, it is indicated with a message displayed at the top of the page.
Provide Feedback