Snapshot value
The
Snapshot value
group contains the following point attributes:Use this attribute | To |
|---|---|
Value | View the current value of the tag, which is based on the tag type. |
Timestamp | View the current time and date of the current tag value. |
These attributes do not contain any data when you are creating a new point.
Provide Feedback