System connectivity
While setting up the FactoryTalk Historian ME environment, pay attention to the following guidelines:
This value | Is the maximum number of |
|---|---|
2 | Modules per chassis. |
10 | Controllers that can transfer data to a single module. There can be a maximum of 5 controllers in the local chassis and a maximum of 5 controllers in the remote chassis. |
50 | Modules that can be used to transfer data simultaneously from the ME to a single SE server. |
5 | Clients that can have simultaneous access to the module. This number includes a web browser, the FactoryTalk Historian SE or PI server, and any other client tool. After the limit is reached, any client will be denied access to the module based on the total number of connections exceeded. |
Provide Feedback