Install the module in the chassis
FactoryTalk Historian ME has the following product number: 1756-HIST2G.
To install the module, follow the
FactoryTalk Historian Machine Edition Module
Installation Instructions (Publication 1756-IN106)
.FactoryTalk Historian ME receives data from the ControlLogix data collection interface and stores it locally in the module. The module data and system information can be viewed and managed through the FactoryTalk Historian ME web page.
After you install the module, you can log on to the FactoryTalk Historian ME web page. See Log on to FactoryTalk Historian ME for details.
Provide Feedback