Prepare the module for the upgrade or reinstallation

To prepare the module for the upgrade or reinstallation
  1. In the module web interface, stop the following services:
    • The data collection (
      Configure Historian > Data Collection
      ).
    • The data transfer (
      Configure Historian > Data Transfer
      ).
  2. Open the web browser, and type
    https://<ModuleIP_address>:8443
    . The module Web Diagnostics interface appears.
  3. Record the firmware version number from the
    Home
    page.
  4. (optional) Click
    Admin > Download Logs
    to download all log files.
  5. Identify the network path across the backplane in the local chassis from the network module to FactoryTalk Historian ME as defined in
    RSLinx® Classic
    . This is not the path through the front port of the module. To view the network path across the backplane, see the image in step 4 in Upgrade or reinstall the module's firmware.
  6. Log out and disconnect all clients (including web clients).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal