Verify time synchronization

To verify time synchronization
  1. Open the web browser and type
    https://<Module IP_address>:8443
    .
    The FactoryTalk Historian ME Web Diagnostics client appears.
  2. Click the
    Hardware
    tab, and then click
    Time Management
    .
    The
    Time Management
    page appears.
  3. Under
    Time Management
    , verify the settings for the NTP server computer.
If there are any problems with the synchronization, an error message appears next to the
Time Source
box.
Verify time synchronization
The time synchronization status is additionally indicated by:
You can find additional details about the synchronization under
NTP Logs
.
Time Management
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal