Battery clock
The Historian module's real-time clock is maintained by the replaceable lithium
battery.
The battery is non-rechargeable and field-replaceable. It powers the real-time clock for two years when the module is not powered on and for twelve years with power to the module on.
For information on replacing the battery, see the
FactoryTalk Historian Machine Edition
Module Installation Instructions (Publication 1756-IN106)
.Provide Feedback