Restart the module

To restart the module
  1. Shut down the module.
  2. Click the
    Advanced
    tab, and then click
    Module Shutdown
    .
  3. Go to the module, and do either of the following:
    • Cut off and restore the power to the module by turning off and on the power switch on the chassis.
    • Unplug and insert the module to the chassis.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal