Snapshot and archive

Click the
Snapshot and Archive
option to view the current FactoryTalk Historian ME snapshot and archive statistics.
Snapshot and archive
The
Snapshot And Archive
section displays the following information:
Item
Description
Type
The snapshot or archive file type.
Counter
The performance counter. For details, see Snapshot and archive counters.
Value
The current snapshot and/or archive value.
Change
The value change between updates.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal