System status

System status
The
System Status
section displays the following information:
This item
Displays
Point Server
FactoryTalk Historian ME server that manages the archives and provides access to historical data. The status may be Running or Error.
Data Collection Service
FactoryTalk Historian ME data collection subsystem. The status may be Running, Stopped, or Error.
Data Transfer Service
FactoryTalk Historian ME data transfer subsystem. The status may be Running, Stopped, or Error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal