Network settings

Network settings
The
Network Settings
section displays the following information:
This item
Displays
MAC Address
The Unique Media Access Control (MAC) address of the module.
This number cannot be changed.
IP Address
The Internet Protocol (IP) address of the module.
IP Configuration
The Dynamic Host Configuration Protocol (DHCP) or static IP address will display. DHCP is the default configuration.
Link Status
The current connection status of the module's front Ethernet port.
TIP:
To change the network settings, click the
Advanced
tab, and then click
System Settings
. For details, see Configure system settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal