Client connections

The
Client Connections
section displays the number of clients currently connected to FactoryTalk Historian ME. There may be up to five clients connected simultaneously to the Historian module.The following client applications are supported:
- FactoryTalk Historian DataLink
- FactoryTalk Historian ProcessBook
- FactoryTalk View SE Trending
- FactoryTalk Administration Console
- PI System Management Tools (SMT)
- FactoryTalk VantagePoint
- FactoryTalk VantagePoint EMI
Provide Feedback