Display the vertical bar on the trend

Use the
Show Vertical Bar
option to display a vertical bar across all points on the X axis. At the bottom of the trend, timestamps will be adjusted when you click inside the trend and drag the vertical bar across it.
To display the vertical bar on the trend
  1. Click Display points on the trend.
    The button color changes to grey (Zoom the trend). The data on the trend is no longer refreshed.
  2. Select the
    Show Vertical Bar
    option next to the trend.
    When you move the mouse pointer over the trend, a vertical bar moves along with the pointer.
  3. Click View trends (2).
    Display the vertical bar on the trend (2)
    TIP:
    When Daylight Savings Time (DST) occurs, the timestamps displayed will be automatically updated to reflect the time change. If you adjust the start time to an earlier start time, the timestamps reflected will coincide with DST even if the DST transfer did not occur until later.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal