Display points on the trend

Use the
Show Points
option to display individual points on the trend.
To display points on the trend
  1. Click Display points on the trend.
    The button color changes to grey (Zoom the trend). The data on the trend is no longer refreshed.
  2. Select the
    Show Points
    option next to the trend.
    Individual points are displayed on the trend as small circles.
  3. Click View trends (2).
    Display points on the trend (3)
    TIP:
    If you want to draw a trend chart that consists of high-speed points, avoid selecting the
    Show Points
    option due to the large number of points that will be displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal