Refresh views
You can refresh the content of the search results table either manually or automatically.
To refresh the search results table manually
- ClickSearch.
To refresh the search results table automatically
- Below the table, in theAuto Refreshbox, type a refresh interval in seconds.
When using the
Auto Refresh
option, note the following:- It is recommended that you turn off the option if you do not need it.
- Display the minimum amount of data necessary to reduce memory consumption.
- Choose the refresh rate prudently. The faster the auto-refresh frequency is, the more memory it consumes.
- Turn the auto refresh option off before closing the web browser or opening another page to release the memory that was being used.
Provide Feedback