Arrange columns

Use the following options to arrange columns and their content.
To change the sorting order in a column
  1. Move the mouse pointer over a column heading.
    An arrow at the top of the column heading indicates its current sorting order:
    Item
    Description
    Ascending arrange columns
    The sorting order is ascending.
    Descending arrange columns
    The sorting order is descending.
  2. Click the column heading to change the sorting order.
    TIP:
    To reduce the load on the FactoryTalk Historian ME processor, sorting occurs on the client computer. If you are monitoring your processor through the task manager, you may see increased processor usage due to the sorting.
To select columns to display
  1. Move the mouse pointer over a column heading.
    A down arrow appears next to the heading.
  2. Click the arrow to list available table columns.
    • To add a column to the table, select the checkbox next to the column that you want to add.
    • To remove a column from the table, clear the checkbox next to the column that you want to remove.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal