Bad quality data
FactoryTalk Historian ME tracks data quality during the data collection and the data transfer. It may happen that data is of bad quality (for example, if the controller loses its connection to the FactoryTalk Historian ME, or if a running tag is removed from the controller but not from FactoryTalk Historian ME).
Bad quality data is displayed in the point list with the
Bad_Quality
value.Provide Feedback