View the default point discovery rule file

By default, FactoryTalk Historian ME provides a point discovery rule file named
ADDefault.xml
. It contains search criteria with which you find tags for the point creation process.
The path to the
ADDefault.xml
file is the following:
<Program Files (x86)>\Rockwell Software\FactoryTalk Historian ME\ME Rule Editor\ADDefault.xml
You can open the file from the Rule Editor, or in an XML editor.
To view the default rule file in the Rule Editor
  1. Go to
    Start > All Programs > Rockwell Software > FactoryTalk Historian ME Rule Editor > Launch Rule Editor
    .
    The FactoryTalk Historian ME Rule Editor window appears.
  2. Under
    File Management
    , click
    View XML file
    .
    The file is displayed in your web browser.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal