Web client issues
Symptom | Solution |
|---|---|
You cannot access the FactoryTalk Historian ME web client. | First check that the IP address you are trying to connect to is the same as the
one scrolling across the FactoryTalk Historian ME module's display. If you see a
MAC address instead, that means that the module can't find the IP address from the
DHCP server. Restart the module. |
The web client is unresponsive. | In the Logix Designer Module Profile, in the Configuration tab, click Restore Defaults . |
You can access the FactoryTalk Historian ME web client but cannot log on. |
|
The administrator forgot the login name and/or password. |
|
You are using the host name as a URL and cannot access the web client. |
|
The web home page is slow to respond. |
|
Provide Feedback