Hardware issues
Symptom | Solution |
|---|---|
The FactoryTalk Historian ME module display is not responding. |
|
The time displayed on the web client is wrong, even if the clock time has already been synchronized in manual mode. | The battery may need to be replaced. The battery is non-rechargeable and field-replaceable. For information on replacing the battery, see the FactoryTalk Historian Machine Edition Module Installation Instructions (Publication 1756-IN106) . |
The four-character LED display stops scrolling. |
|
The Ethernet port lights are not illuminated. |
|
The module's CPU is experiencing continuous high usage (90-100%). | Go to the Web Diagnostics Hardware tab, and check the CPU, RAM page to
find out each service's usage and determine which processes are the most
CPU-intensive. |
The FactoryTalk Historian ME module cannot obtain an IP address from a DHCP server. |
|
The MAC address scrolls across the display. |
|
The ME module is online but you cannot access it through its host name. | The FactoryTalk Historian ME module host name may have a "_" in its name.
According to Microsoft DNS server naming standards, this help prevents the module
from being recognized by its host name. To solve this problem, the underscore "_"
must be removed from the module's name. For details on naming the ME module, see Change the module name. For details on DNS naming standards, see the Microsoft TechNet site and search for "DNS naming standards". |
Provide Feedback