Create trusts for the data transfer
To ensure a secure connection between FactoryTalk Historian ME and FactoryTalk Historian SE, you need to create the following trusts in System Management Tools on the FactoryTalk Historian SE server:
- A trust forwebs.This trust is required so that you can select points for the data transfer on your Historian ME webpage.When configuring the trust, provide the following information:
- The IP address of your Historian ME module.
- The trust name:webs.
- The trust type:PI-API application.
- The application name:webs.
- A PI user as the PI Identity.
- A trust fordatatransfer.This trust is required so that the selected points are transferred to FactoryTalk Historian SE.When configuring the trust, provide the following information:
- The IP address of your Historian ME module.
- The trust name:datatransfer.
- The trust type:PI-API application.
- The application name:datatransfer.
- A PI user as the PI Identity.
For other data transfer prerequisites, see Data transfer prerequisites.
For details on creating trusts in System Management Tools, refer to the System Management Tools and FactoryTalk Historian SE user documentation.
Provide Feedback