Configure system timeout

If the administrator session expires, you will be automatically logged out and taken to the
Home
tab. The default expiration time is 20 minutes. Configure the value in the
Configure Historian
tab as needed.
To configure system timeout
  1. Click the
    Configure Historian
    tab, and then click
    System Security
    .
  2. Under
    System Security
    , enter the value in the
    System Timeout
    box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal