Understand privileges for user groups
The following table displays the privileges for user groups configured in the FactoryTalk Historian ME Module or on the FactoryTalk Directory server in the FactoryTalk Administration Console.
Depending on the way you log on to the module, you will have different user groups at your disposal, and you will manage them differently:
- If you are using FactoryTalk Historian ME Local Security credentials, you can manage the user groups on theGroup Managementpage.For details, see View groups.
- If you are using the FactoryTalk Directory security credentials, you can manage the user groups in the FactoryTalk Administration Console on the FactoryTalk Directory server computer.
If the logon mode is changed, all groups and users associated with the previous logon mode are lost.
Operation | The FactoryTalk Directory security groups | The FactoryTalk Historian ME Local Security groups | ||||
|---|---|---|---|---|---|---|
FTHAdministrators | FTHEngineers | FTHSupervisors | FTHOperators | piadmin | piuser | |
Manage SNMP | Yes | No | No | No | Yes | No |
Create tag | Yes | Yes | No | No | Yes | No |
Read status | Yes | Yes | Yes | Yes | Yes | Yes |
Start data collection | Yes | Yes | Yes | No | Yes | No |
Stop data collection | Yes | Yes | Yes | No | Yes | No |
Read point definition | Yes | Yes | Yes | Yes | Yes | Yes |
Modify point properties | Yes | Yes | No | No | Yes | No |
Read point historical data | Yes | Yes | Yes | Yes | Yes | Yes |
Export point historical data | Yes | Yes | Yes | Yes | Yes | Yes |
Read system log | Yes | Yes | Yes | Yes | Yes | Yes |
Read user information | Yes | Yes | Yes | Yes | Yes | Yes |
Create/modify/delete user | Yes | No | No | No | Yes | No |
Change password (self) | Yes | Yes | Yes | Yes | Yes | Yes |
Change password (other users) | Yes | No | No | No | Yes | No |
Read group information | Yes | Yes | Yes | Yes | Yes | Yes |
Create/modify/delete group | No | No | No | No | Yes | No |
Create/modify/delete trust | Yes | No | No | No | Yes | No |
Save NTP server | Yes | Yes | No | No | Yes | No |
Synchronize time | Yes | Yes | No | No | Yes | No |
Read backup status | Yes | Yes | Yes | Yes | Yes | Yes |
Backup configuration | Yes | Yes | No | No | Yes | No |
Download backup file | Yes | Yes | No | No | Yes | No |
Upload backup file | Yes | Yes | No | No | Yes | No |
Restore configuration | Yes | Yes | No | No | Yes | No |
Reset module | Yes | Yes | No | No | Yes | No |
Reset security | Yes | Yes | No | No | Yes | No |
Read security mode | Yes | Yes | Yes | Yes | Yes | No |
Change security mode | Yes | Yes | No | No | Yes | No |
Change protocol | Yes | Yes | No | No | Yes | No |
Manage shortcuts | Yes | Yes | No | No | Yes | No |
Provide Feedback