Rename points

To rename points
  1. Click
    Manage Points
    , and then click
    Edit Points
    .
    The
    Edit Points
    page appears.
  2. Using the search boxes, set your point search criteria, and then click
    Search
    .
  3. In the search results table, click the point that you want to edit, and then click
    Rename
    .
    The
    Point Property
    page appears.
  4. Change the point name.
    If you want to cancel your changes and bring back the original attributes of the point, click
    Reset
    .
    TIP:
    Resetting will not work after you save the changes using the
    Save
    button.
  5. Click
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal