Edit points
To edit points
- ClickManage Points, and then clickEdit Points.TheEdit Pointspage appears.
- Using the search boxes, set your point search criteria, and then clickSearch.
- In the search results table, click the point that you want to edit, and then clickEdit.ThePoint Propertypage appears.
- Change the point attributes.For details, see Define point attributes.If you want to cancel your changes and bring back the original attributes of the point, clickReset.TIP:Resetting will not work after you save the changes using theSavebutton.
- ClickSave.
Provide Feedback