Create points

To create points
  1. Click
    Manage Points
    , and then click
    Edit Points
    .
    The
    Edit Points
    page appears.
  2. At the bottom of the page, click
    New
    .
  3. The
    Point Property
    page appears.
  4. Fill in the point attributes.
    For details, see Define point attributes.
  5. Click
    Save
    .
If the data transfer service is set to the auto transfer mode, the new points will be created with the new tag names automatically. Otherwise, you need to add the new points to the data transfer manually.
To add new points to the data transfer
  1. Click
    Configure Historian
    , and then click
    Data Transfer Points
    .
    The
    Data Transfer Points
    page appears.
  2. Using the search boxes, find the points that you want to add to the data transfer.
  3. In the search results table, select the points that you want to add to the data transfer.
  4. Click
    Save
    .
  5. In the left pane of the window, click
    Data Transfer
    .
  6. Restart the data transfer service.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal