Edit scan classes

TIP:
You must have administrator privileges to edit scan classes.
To edit a scan class
  1. Click
    Manage Points
    , and then click
    Edit Scan Class(es)
    .
  2. In the table, select the scan class that you want to edit.
  3. At the bottom of the page, click
    Edit
    .
  4. At the top of the page, in the
    Time
    text box, change the scan rate value.
  5. Click
    Save
    .
  6. Click
    OK
    to close the dialog box, and then click
    Restart
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal